SPRUIZ2 july 2023 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The CMPSS module on F28P65x has been updated to support the Diode Emulation Logic (DEL). The CMPSS module in F2838x includes a ramp generator with ramp up capability. The CMPSS module in F28P65x ramp generator supports both ramp up and ramp down of the local CMPSS DAC. The digital filter in the F28P65x CMPSS now also has an option to use it with an external source. Consult F28P65x CMPSS chapter in the TRM for more details on the new features.