SPRUIZ2 july 2023 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
F2838x does not have an internal VREG and only external VREG is supported. F28P65x supports internal and external VREG and is selectable using the VREGENZ pin. VREGENZ pin in F28P65x has an internal pullup which defaults the operation in external VREG mode on the VDD pin if pin is left floating. VREGENZ pin location in F28P65x is a NC (no connect) pin in F2838x devices.