SPRUIZ2 july 2023 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Section 2.2.3.1 outlines the GPIO number and the corresponding peripheral multiplex pin functions of certain pin positions that changed from F2838x to F28P65x. Most of the peripheral functions on these pin positions were retained for both devices, with the exception of a few, as shown on the table. Examples below illustrate how to account for the GPIO number and peripheral function changes:
Section 2.2.3.2 outlines the ADC channels that will take the position of ADCD module when moving from F2838x to F28P65x. Change the ADC channel setup accordingly depending on which function/channel assignment is allocated based on the table