The buttons initialize different
phases of the power estimation.
- Reset clears and resets the
form as well as clearing results.
- Populate Use Case – Start any
power estimate by using one of the pre-configured representative use cases.
This helps to highlight how the tool can be used in a reasonable way (i.e.,
do not enter 100% for all of the IP on the SoC).
- Calculate – once the form is
completed, calculate to populate data into the results sheet.
- Save current UC – once the
user gets a test case competed, the case can be saved if a UC Name has been
supplied. Once saved with a unique name, the case is part of the “Starting
Use Case” list and is re-populated with the populate use case button. One
particular note about re-populating use cases involves the SerDes and
Display Sub-System. A SerDes bandwidth cannot map to the driving IP. As an
example, an 8G Lane can be driven by the DSS or PCIe GEN 3. The user must,
therefore, configure the SerDes IP and define what outputs the DSS is using.
The tool applies loading to the IP designated by the SerDes and the DSS
based upon these manual changes.
When each button is pushed, the cells
underneath the button (H8:I11) record the start and stop times.