SPRZ412N December 2013 – May 2024 TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
Figure 2-1 and Figure 2-2 provide examples of the 2837xD device markings and define each of the markings. The device revision can be determined by the symbols marked on the top of the package as shown in Figure 2-1 and Figure 2-2. Some prototype devices may have markings different from those illustrated. Figure 2-3 shows an example of the device nomenclature.
SILICON REVISION CODE | SILICON REVISION | REVID(1) Address: 0x5D00C |
COMMENTS |
---|---|---|---|
Blank | 0 | 0x0000 | This silicon revision is available as TMX. |
A | A | 0x0000 | This silicon revision is available as TMX. |
B | B | 0x0002 | This silicon revision is available as TMX. |
C | C | 0x0003 | This silicon revision is available as TMS. |