Revision
History
Changes from December 31, 2023 to December 11, 2024 (from Revision A (December 2023) to Revision B (December 2024))
- Added Usage Note i2424; PLL: PLL Programming Sequence May Introduce
PLL InstabilityGo
- Added Advisory i2376; C7x: SE/SA/HWAOPEN receives corrupted template
following two back to back VPUT/MVC instructionsGo
- Added Advisory i2399: C7x: CPU NLC Module Not Clearing State on
InterruptGo
- Added Advisory i2413: Boot: HS-FS ROM boots corrupted ROM boot
imageGo
- Added Advisory i2414: Boot: Ethernet PHY Scan and Bring-Up Flow
doesn't work with PHYs that don't support Auto NegotiationGo
- Added Advisory i2419: Boot: When disabling deskew calibration, ROM
does not check if deskew calibration was enabledGo
- Added Advisory i2420: Boot: XSPI Boot time is not consistent in SFDP
modeGo
- Added Advisory i2421: Boot: fatTiny GPT handling causes data
abortGo
- Added Advisory i2422: Boot: ROM timeout for MMCSD filesystem boot
too longGo
- Added Advisory i2423: Boot: HS-FS ROM applies debug access
restrictions to all address space covered by the efuse controller
firewallGo
- Added Advisory i2431; BCDMA: RX Channel can lockup in certain
scenariosGo
- Added Advisory i2435: Boot: ROM timeout for eMMC boot too
longGo