SWCU193A April 2023 – August 2024 CC2340R2 , CC2340R5 , CC2340R5-Q1
There are four conversion modes available in the ADC:
The following steps outline the recommended process for configuring the ADC for a desired conversion mode:
Software Trigger | Event Trigger | |
AUTO Sampling Mode |
For repeat and sequence modes, if TRIG is set in MEMCTL, the SC bit needs to be set for the next conversion to proceed. |
For repeat and sequence modes, the ADC waits for the EVENT trigger or automatically starts the next conversion based on the TRIG setting. |
MANUAL Sampling Mode |
Repeated/sequential conversion modes are NOT supported in this configuration. | ADC operation is NOT supported in this configuration. |