SWCU193A April 2023 – August 2024 CC2340R2 , CC2340R5 , CC2340R5-Q1
A channel can be armed in Capture mode by setting the SYSTIM.CHnCFG[0] MODE bit to 1.
In Capture mode, the channel captures the 32 bits of SYSTIM time based on the event that the channel receives. The resolution of these 32 bits is based on the type of channel used. The capture can be configured on different edges of the input event. For more details, refer to the SYSTIM.CHnCFG register.
By default, a channel is disarmed after capture happens. The SYSTIM.CHnCFG[0] MODE bit is cleared to 0.