SWRA601L April 2019 – October 2024 CC1350 , CC1352P , CC1352P7 , CC1352R , CC2340R5 , CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R , CC2642R-Q1 , CC2650 , CC2650MODA , CC2652P , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP
In general, you are not expected to modify the Core Layers supported by the design. Such modification triggers requirements for testing that cannot be achieved with the software publicly provided by TI.
Systems integrators usually want to modify the list of GATT Profiles and Services supported by the design – this is what is described in the steps below:
The Consistency Check tool indicates if capabilities checkboxes are inconsistent with other capabilities checked, or missing mandatory capabilities. In case the TCRL referenced for the design is different from the TCRL referenced when TI obtained the DN, some inconsistencies within the core layers (GATT, LL, and so forth) may be reported. These inconsistencies are expected. The Test Coverage Waiver (TCW) [28]. ES-25636 should be applied to waive the inconsistencies and proceed with the qualification process for the product.
Similarly, the ICS selection for the Core Specifications is expected to be left untouched. Only the added ICS selection for the added GATT Profiles and Services should be reviewed and modified if needed.