SWRA705 August 2021 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR2944 , AWR6443 , AWR6843 , AWR6843AOP , AWRL1432 , AWRL6432 , IWR1443 , IWR1642 , IWR1843 , IWR2243 , IWR6243 , IWR6443 , IWR6843 , IWR6843AOP , IWRL6432 , IWRL6432AOP
The wall thickness of the radome plays a key role in arriving at the optimum performance of the mmWave radar sensor. It is important to make sure that the radome wall thickness is equal to an integer multiple of the radar wavelength/2 so that the radome becomes “nearly transparent” for the mmWave frequency range intended. The thickness of radome is given in Equation 3. The wavelength in the radome material becomes shorter versus free air and is an inverse function of the material's dielectric constant as shown in Equation 4.
Where,
In general, radome performance depends mainly on the frequency of use, thickness, εr, incident angle, and shape. For the normal incident case, optimum thickness given in Equation 4 is plotted in Figure 2-4 and Figure 2-5.