SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3350 , CC3351
Because it is important to reduce the current consumption of the device, CC33xx features an extreme low power (ELP) level that is used in many of the power saving modes described below. ELP is a device power state during which the device sleeps to drastically decrease power consumption in between activity. This device enters this state as required by the Wi-Fi power management protocols described below.