SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3301MOD , CC3350 , CC3351
The keep alive feature works in conjunction with the features described below to ensure that when the CC33xx acts as a station it retains connection to APs during periods of no activity. As part of many of the protocols, the device is inherently not required to transmit any data back that can cause an AP to think that it is an inactive device. To account for this, the keep alive feature is automatically implemented in parallel to the below protocols.
If, after 55 seconds, the CC33xx has not transmitted any traffic to the AP, the device sends a null frame. This null frame informs the AP that the station is still active and should not be forced off the network.