SWRU616B September 2023 – April 2024 CC3300 , CC3301 , CC3350 , CC3351
When this mode is enabled, the unprovisioned CC33xx device is initially set-up as an AP with a pre-defined SSID. While the CC33xx device is operating as an AP, the user can connect and enter the required credentials. Once the security credentials have been entered, the device switches from AP mode to STA mode and connect to the network using those previously provided credentials.