The following steps are used for the test setup:
- If the UCD3138 control card is new, flash the
code into the card (skip this step if the card is pre-flashed)
- Insert the UCD3138 control card and the auxiliary power board into the base board
- Connect the input DC source and output electronic load
- Consider using an extra cooling fan to minimize the temperature of the power board
- Power on the DC source with 400 V, the 12-V output automatically starts up