The Device Configuration
allows users to configure the devices' setting as shown in Figure 3-12.
- Configuration register can be set to desired values
by selecting the drop-down menu.
- Non-volatile memory can be programmed by entering the
value at the EEPROMx boxes. Then use the EEPROM
dropdown menu to lock the value. This LOCK bit will
also lock the value of the offset temperature
register.
- Alert High and Low Limit register can be set by
entering the value in °C/°F. In Fahrenheit mode, it
converts Fahrenheit to Celsius before it sends to
the TMP117.
- Status indicator displays the outputs based on the
status bits.
- Temperature displays the current temperature of the
TMP117.
- Offset Temperature programs the offset temperature to
compensate and improve the system error. This
register will be cleared when powered down unless
the LOCK is set.