Firefox is a trademark of Mozilla Foundation.
Google Chrome is a trademark of Google LLC..
All other trademarks are the property of their respective owners.
The ADS7038-Q1 EVM is a fully-assembled evaluation platform designed to highlight the ADS7038-Q1 features and various modes of operation that make this device suitable for ultra-low-power, small-size sensor monitor applications. The accompanying Precision ADC Motherboard (PAMBoard) development kit is used as a USB-to-PC GUI communication bridge. This kit also serves as an example implementation of a master microcontroller (MCU) to communicate with the ADS7038-Q1 device through a serial-peripheral interface (SPI).
The ADS7038-Q1 EVM requires an external master controller to evaluate the ADS7038-Q1 device.
The PAMBoard is controlled by commands received from the ADS7038-Q1 GUI, and returns data to the GUI for display and analysis. If the PAMBoard is not used, the EVM plug-in module format allows for an alternative external host to communicate with the ADS7038-Q1 by easily connecting through a pin header. The ADS7038-Q1 device incorporates all required circuitry and components with the following features:
ADS7038-Q1 small general purpose, feature integrated, eight-channel ADC
Buffered analog input drive circuit available on channel 0
External power-supply connection available to provide DVDD power supply instead of the USB power
Adjustable linear regulator, TPS78001, to generate stable output voltage to AVDD from the 5-V USB power from the PAMBoard
SPI for communication and configuration of modes
Figure 1-1 shows the ADS7038-Q1EVM input circuity for the analog inputs.