SFFS022 December 2022 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
This document is the Functional Safety Manual for the TMS320F2838xD/S MCU series from Texas Instruments which is part of the high performance C2000™ real-time microcontroller product line. The TMS320F2838xD device is based on a dual core CPU architecture with a C28x CPU for each core. Each C28x CPU is referred as CPU1 and CPU2 respectively. In addition, this device contains a connectivity manager based on an Arm® Cortex® M4 CPU. The connectivity manager safety related topics are beyond the scope of this safety manual. The C2000 product line utilizes a common safety architecture that is implemented for multiple products in automotive and industrial applications.
C2000™ is a trademark of Texas Instruments.
Arm® and Cortex® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
EtherCAT® is a registered trademark of and licensed by Beckhoff Automation GmbH.
All trademarks are the property of their respective owners.
The products supported by this document have been assessed to be meet a systematic capability compliance of ASIL-D (according to ISO 26262) and SIL-3 (according to IEC 61508). For more information, see the Texas Instrument's functional safety hardware development process.
This Functional Safety Manual is part of the Functional Safety-Compliant design package to aid customers who are designing systems in compliance with ISO26262 or IEC61508 functional safety standards.
Table 1-1 shows a complete list of the products supported by this safety manual (including silicon revision A) and the part numbers.
Orderable Devices | |
---|---|
Dual-Core Part Numbers | Single-Core Part Numbers |
TMS320F28384DZWTS | TMS320F28384SZWTS |
TMS320F28386DZWTS | TMS320F28386SZWTS |
TMS320F28388DZWTS | TMS320F28388SZWTS |
TMS320F28388DZWTSR | TMS320F28388SZWTSR |
TMS320F28388DPTPS | TMS320F28388SPTPS |
TMS320F28388DPTPSR | TMS320F28388SPTPSR |
TMS320F28386DPTPS | TMS320F28386SPTPS |
TMS320F28384DPTPS | TMS320F28384SPTPS |
TMS320F28386DPTPQ | TMS320F28386SPTPQR |
TMS320F28386DPTPQR | TMS320F28384SPTPQR |
TMS320F28384DPTPQR | – |
TMS320F28386DZWTQ | – |
TMS320F28386DZWTQR | – |
TMS320F28384DZWTQR | – |
This Functional Safety Manual provides information needed by system developers to assist in the creation of a safety critical system using a supported TMS320F2838x MCU. This document contains:
The following information is documented in the Detailed Safety Analysis Report (SAR) section of the FMEDA, for TMS320F2838x C2000™ Safety Critical Microcontrollers, which is only available under a Functional Safety NDA and is not repeated in this document:
It is expected that the user of this document should have a general familiarity with the TMS320F2838x product families. More information can be found at www.ti.com/C2000.
This document is intended to be used in conjunction with the pertinent data sheets, technical reference manuals, and other documentation for the products being supplied.
For information which is beyond the scope of the listed deliverables, please contact your TI sales representative or www.ti.com.