SFFS293 September 2021 TPSM82821 , TPSM82821A , TPSM82822 , TPSM82822A , TPSM82823 , TPSM82823A
All trademarks are the property of their respective owners.
This document contains the Pin failure mode analysis (pin FMA) information for the TPSM82821, TPSM82822, TPSM82823, TPSM82821A, TPSM82822A, and TPSM82823A (uSiP package).
Figure 1-1 shows the device functional block diagram for reference.
The TPSM8282x was developed using a quality-managed development process, but was not developed in accordance with the IEC 61508 or ISO 26262 standards.
This section provides a failure mode analysis (FMA) for the pins of the TPSM8282x. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 2-2 through Table 2-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 2-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality. |
B | No device damage, but loss of functionality. |
C | No device damage, but performance degradation. |
D | No device damage, no impact to functionality or performance. |
Figure 2-1 shows the TPSM8282x pin diagram. For a detailed description of the device pins, see the Pin Configuration and Functions section in the TPSM8282x data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN | 1,2 | Device will not be powered up | A |
EN | 3 | Device will not be enabled | B |
PG | 4 | Loss of PG functionality | B |
VOUT | 5,6,7 | Device not functional | A |
FB | 8 | Output voltage will not be regulated. Device will enter 100% mode. | B |
GND | 9,10 | Intended functionality | D |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN | 1,2 | Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance | C |
EN | 3 | Undetermined state of the pin; device may or may not be enabled | B |
PG | 4 | Loss of PG functionality | B |
VOUT | 5,6,7 | Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance | C |
FB | 8 | Device not functional; Open loop operation | B |
GND | 9,10 | Redundant pin. If one of the pins are open, no functionality loss but potential impact on device performance | C |
Pin Name | Pin No. | Shorted to | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|---|
VIN | 2 | EN | 3 | Loss of Enable functionality | B |
EN | 3 | PG | 4 | Loss of Enable functionality; Potential device damage | A |
PG | 4 | VOUT | 5 | Loss of PG functionality; Potential device damage | A |
VOUT | 7 | FB | 8 | For adjustable versions output voltage will be regulated to 0.6V (Intended functionality for Fixed Vout devices) | B |
FB | 8 | GND | 9 | Output voltage will not be regulated. Device will enter 100% mode. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VIN | 1 | Intended functionality | D |
EN | 3 | Loss of Enable functionality | B |
PG | 4 | Loss of PG functionality; Potential device damage | A |
VOUT | 5,6,7 | Potential device damage | A |
FB | 8 | Device not functional; Open loop operation | B |
GND | 9,10 | Potential device damage | A |