This application note describes using the AFE882H1 in an evaluation module (EVM) to construct a HART®-enabled field transmitter for 4-20mA loop instrumentation. HART (Highway Addressable Remote Transducer) enables two-way digital communication across the current loop at the same time as transmitting the value of a primary process variable. First, a brief introduction to 4-20mA loops and the HART protocol is presented. The AFE882H1 is then introduced as an ultra-low-power, 16-bit digital-to-analog converter (DAC) combined with a HART modem. This device also has an on-board analog-to-digital converter (ADC) and integrated diagnostic sensors for system monitoring. The EVM used for this device is set up as a loop transmitter that sets the current in a 4-20mA loop. This EVM is coupled with a digital back-end board that connects with an MSP-EXP430FR5969 LaunchPad™ as the controller for the HART communications. Testing for this transmitter for HART registration is also presented. The physical layer test results for the waveform are described and the data link layer (DLL) test results for the HART signaling and timing are described. Application layer tests for HART universal commands (UAL) and commonly-implemented commands (CAL) are also described.
LaunchPad™ is a trademark of Texas Instruments.
HART® is a registered trademark of FieldComm Group, Inc.
Linux® is a registered trademark of Linus Torvalds.
All trademarks are the property of their respective owners.