This is the user's guide for the evaluation module (EVM) of the TUSB2E11 single channel eUSB2 to USB 2.0 repeater. The purpose of the user's guide is to facilitate easy set up for validation and development of the TUSB2E11 device. An overview of the TUSB2E11EVM is provided in this user’s guide, which includes highlighting its key features, operating conditions, and how to adjust the EVM for use in various systems.
All trademarks are the property of their respective owners.