Parameter | Design Requirement | ||
---|---|---|---|
Supply voltage | ±12 V | ||
Output voltage | 1.25 V | ||
Output current | 1 mA | ||
Output noise | < 25 nV/√Hz from 1 kHz to 10 MHz | ||
Radiation hardness | 50 kRad(Si) |
This circuit design uses a low-pass filter and an op amp to reduce the wideband noise generated by a shunt voltage reference. The circuit was originally developed to supply a CCD sensor in a satellite: the shunt reference alone does not meet the performance requirements of the application and needs the additional circuitry to meet the project requirements.
TI has a number of suitable space-qualified voltage references, but for this application the TL1431-SP was selected for its good noise performance and high radiation tolerance. The lowest voltage that U1 can generate is 2.5 V, so R2 and R3 are used to generate a 1.25-V input to U2 (they also attenuate the noise of U1 by a factor of two). Low values are used for R1 and R2 to limit the noise generated by these components. R1 is chosen so that, even with R2 and R3 connected, there is 1 mA of bias current through U1.
R4 and C1 form the low-pass filter that attenuates noise from the voltage reference. With the values shown, the 3-dB frequency of this filter is 145 Hz. The precise values of R4 and C1 are not critical. However, it pays not to make R4 too large, because the op amp has to correct any errors caused by the output current flowing through R4, and if the voltage drop across R4 is too large the op amp may run out of headroom.
R4 and C1 add a pole to the amplifier response; R5 and C2 add a zero that compensates this pole and enables stable operation. R5 and C2 are chosen so that R5 × C2 = 2 × R4 × C1, which minimizes noise gain peaking in the response.
The op amp used for this application should not itself generate significant noise compared to the voltage reference; however, the filter formed by R4 and C1 attenuates whatever noise the op amp does generate. Note that in the case of the OPA4277-SP, with the component values used, current noise is insignificant compared to voltage noise and can be ignored.
Use the following equation to calculate the maximum value of R1:
A value of 3.9 kΩ is therefore suitable for R1.
Use the following equation to calculate the RC time constant needed for the desired cutoff frequency:
Using values of R4 = 110 Ω and C1 = 10 μF results in a cutoff frequency of 145 Hz.
Simulation Setup
The easiest way to analyze the noise performance of a circuit like this is to use a simulation program such as TINA.
The SPICE macros for the TL431 and OPA4277 included in the standard TINA library(1) do not include models for the noise performance, so separate voltage noise sources must be included in the simulation circuit (see Vn1 and Vn2 in the previous TINA schematic). The macros for the noise sources can be copied from the Vnoise.TSC file referred to in this E2E thread, and edited, and three parameters describing the noise characteristic of the devices entered (highlighted in bold in the following macro extract).
* BEGIN PROG NSE NANO VOLT/RT-HZ
.SUBCKT VNSE 1 2
* BEGIN SETUP OF NOISE GEN - NANOVOLT/RT-HZ
* INPUT THREE VARIABLES
* SET UP VNSE 1/F
* NV/RHZ AT 1/F FREQ
.PARAM NLF=225
* FREQ FOR 1/F VAL
.PARAM FLW=10
* SET UP VNSE FB
* NV/RHZ FLATBAND
.PARAM NVR=125
* END USER INPUT
* START CALC VALS
.PARAM GLF={PWR(FLW,0.25)*NLF/1164}
.PARAM RNV={1.184*PWR(NVR,2)}
.MODEL DVN D KF={PWR(FLW,0.5)/1E11}IS=1.0E-16
* END CALC VALS
I1 0 7 10E-3
I2 0 8 10E-3
D1 7 0 DVN
D2 8 0 DVN
E1 3 6 7 8 {GLF}
R1 3 0 1E9
R2 3 0 1E9
R3 3 6 1E9
E2 6 4 5 0 10
R4 5 0 {RNV}
R5 5 0 {RNV}
R6 3 4 1E9
R7 4 0 1E9
E3 1 2 3 4 1
C1 1 0 1E-15
C2 2 0 1E-15
C3 1 2 1E-15
.ENDS
* END PROG NSE NANOV/RT-HZ
NLF is the magnitude of the noise where the curve crosses the y-axis at the minimum frequency, and FLW is the frequency at which this happens. NVR is the magnitude of the wideband noise. These parameters can easily be taken from the data sheets of the devices (see the following figure). All values entered in the macros must be in nV/√Hz.