Shunt regulators of the 431 family (TL431, TL431LI, ATL431 and ATL431LI) behave as a voltage comparator when operated in open loop. Voltage is sensed at the reference pin and output is taken from the cathode pin as shown in Figure 2-1. A shunt voltage reference is commonly used in the feedback loop of the PWM controllers in switching power supplies. Shunt regulators are very popular for its low cost and built-in precise reference. It acts as an error amplifier in the feedback loop with the optocoupler. It senses the output voltage and trigger the optocoupler for the PWM controller feedback. This application note explains the comparator mode operation and discusses the key design considerations for the 431 family in the comparator mode.
All trademarks are the property of their respective owners.
The 431 family of TI shunt regulators are used in the comparator mode by opening the DC feedback path, when there is no DC current from cathode to reference pin. Below are examples of circuits for shunt regulators in the comparator mode. Figure 2-1 shows the simple comparator circuit and Figure 2-2 shows the typical type II compensation which is used in isolated power supply designs with optocoupler feedback. This section discusses the specs of the family 431 in comparator mode.
The threshold voltage (VIT) for 431 shunt regulators in comparator mode is equal to the reference voltage of the device. Comparator changes the output state when input crosses VIT level. Table 2-1 lists VIT levels for 431 shunt regulators
Devices | Typical Threshold (VIT) in Comparator Mode (V) |
---|---|
TL431, TL431LI | 2.495 |
ATL431, ATL431LI | 2.5 |
TLV431, TLVH431 | 1.24 |