This application note describes the step-by-step process of building an Edge AI application for vision tasks on TI AM6xA processors, using the AM62A and a retail-scanner demo to provide an example of the process. Following this development flow greatly accelerates new designs. This document details the TI Processor-specific steps for training, compiling, and running a model. Additionally, this document provides information about creating a gstreamer pipeline in Linux that leverages hardware accelerators for image processing such that the developer need not program those accelerators manually.
All trademarks are the property of their respective owners.
The purpose of this document is to describe the tools and process for creating an Edge AI Vision application for Texas Instruments AM6xA Microprocessors. The exemplary application uses the AM62A for an automated retail scanner or checkout system, in which a customer’s tray of food items is quickly and automatically recognized using a deep learning neural network, accelerated by TI’s C7xMMA deep learning accelerator.
This application note follows the overall development flow as shown in Figure 1-1, starting from a custom dataset and a partially trained model from the TI Model-Zoo [1]. A neural network model is trained with TI-supported tools and compiled to the target device’s C7xMMA architecture. This is then used alongside Gstreamer for developing an end-to-end media pipeline, including camera capture, preprocessing, deep learning inference, post-processing, and display to a monitor. The end application is written in Python3, and open source code can be found online on the Texas Instruments Github under the retail-shopping directory [2]. For instructions on how to run the demo, see the README.md.
This application was developed for AM62A, a quad-core microprocessor from Texas Instruments with 2 TOPS of deep learning acceleration. The model is compiled for this architecture, and will need to be recompiled to run on another TI processor to take full advantage of the accelerator. To learn more about this compilation process, see the related document in TI's Edge AI repo [4] and edgeai-tidl-tools [5]. This application was taken to Embedded World 2023 as a demo to showcase the AM62A.
At the time of implementation, TI’s Model Composer suite of software within the Edge AI Cloud [6] was not yet available for this processor – those tools simplify neural network model development from data capture to model selection to training to compilation and evaluation as shown in Figure 1-1 up through Model Evaluation. This document follows a more programmatic design flow, which offers greater flexibility that experienced developers may prefer.
Find the concept video for the demo on youtube at the following link: https://www.youtube.com/watch?v=jYJvtoPAW6E.
This document is intended for readers with beginner or intermediate level deep learning experience, who aim to bring their ideas onto TI processors for vision applications. It is also intended to help readers add practical knowledge to the implementation of such systems; this document intentionally provides additional tips and comments for those with theoretical understanding but less practical expertise.
For those with minimal deep learning knowledge, it is recommended to follow the Fundamental Concepts pages of the Edge AI Academy [4] in the TI Developer Zone.