SPRUIZ2 july 2023 TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This migration guide describes the hardware and software differences to consider when moving between F2838x and F28P65x C2000™ MCUs. This document shows the block diagram between the two MCUs as a visual representation on what blocks are similar or different. It also highlights the features that are unique between the two devices for all available packages in a device comparison table. To facilitate application and hardware migration between F2838x and F28P65x devices, the PCB hardware section provides guidance on how to proceed with the common 176-pin package. The digital general-purpose input/output (GPIO) and analog multiplex comparison tables show pin functionality between the two MCUs. This serves as a reference for hardware design and signal routing when considering a move between the two devices.
C2000™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
The 176-pin is the only common package between F2838x and F28P65x. It is possible to migrate between F2838x and F28P65x with the caveats in this document taken into account.