Giovanni Campanella and Matthieu Chevrier
To unleash the full potential of Industry 4.0, factories and plants will need to be covered by sensors.
The sheer number of sensors would make wired installations prohibitive, so wireless technologies like wirelessHART and the upcoming Bluetooth® low energy mesh are immediate considerations. The cost of battery replacements for those sensors is often underestimated, however.
Instead of using batteries, powering a sensor from the signal that it is monitoring is a solution for scalability. For example, position or proximity sensors are powered by the actual motion they are monitoring, which enables the system to reach the highest level possible of predictability and robustness.
TI has released a new reference design, the Energy Harvesting for Wireless Switch Power Reference Design, which offers a power management solution for energy harvesting switches (Figure 1). The energy harvesting switch is built like a linear dynamo, transforms mechanical energy into electrical energy. The reference design harvests this electrical energy to enable wireless position control of valves or other mechanical actuators, as well as emergency switches and controllers for machine starts and stops.
The reference design’s application spans factory automation and process control to building automation, as well as nonindustrial areas. You can use this type of solution when you need lower maintenance and installation costs, higher system uptimes and increased flexibility – and when wiring is considered infeasible. In addition, due to the design’s inherent low-power operating characteristics, it is an optimal solution for explosive-proof applications, avoiding the use of expensive protection methods.
When designing an energy-harvesting circuit, the challenge is to extract the maximum amount of energy regardless of the load to have a flexible design reusable across multiple systems.
An electrodynamic system can be a generator with a fixed-output impedance, so in theory, to maximize the energy extraction, you only have to match the source impedance with the load. However, for a dynamically behaving load, this is not possible.
An alternative is to buffer the energy so it can be given as a constant supply to the active load. The challenge is then to be able to still extract as much energy from the generator without exposing a constant load. Two main things should be considered:
Another design consideration to keep in mind is that the generator will generate two pulses: one positive and one negative for each full actuation (push and release). The reference design maximizes energy extraction by going for the rectification of the negative wave.
For the rectification, two options are possible: either a full-wave rectification or a voltage doubler. The reference design follows the voltage-doubler (see Figure 2) option for two reasons:
Finally, the input-cap value as a function of the UVLO voltage was optimized through trial and error with the goal of maximizing the runtime of the DC/DC (that is, the time for which it provides a valid voltage on its output).
The reference design easily interfaces to the SimpleLink™ CC2650 wireless MCU LaunchPad™ kit to transmit wireless data through the CC2650, powered by either the TPS62122 or the TPS62125 present on the board.
The reference design sends out non-connectable advertisement packets on three separate channels that contain 8 bytes of data.
This design could be one of your first steps to unleash your smart factory. Have a look to the schematics, layout and test data on the design page.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated