DLPU103B october 2020 – may 2023 DLP230NP
This section provides instructions for bringing up the DLPDLCR230NPEVM using the Raspberry Pi. It is limited to the basics of installation and communication with the system. Basics of SD card setup for the Raspberry Pi are covered, along with use of the Python API library for the EVM. The function and utility of each sample script in the Python library is also discussed.