DLPU132A October 2023 – March 2024 DLPC964
The Start Page is the first window that users see upon executing the DLPC964 GUI.
This window has the image of a standard setup for the Apps FPGA (AMD EVM) with DLPLCRC964EVM and DLPLCR99EVM.
There are also online resources to help enable customers in getting Evaluation Module Kits started.
If the DLPC964 GUI states that Hardware is not connected, then check: