DLPU133A March 2024 – February 2025 DLPC964
The PGEN (Pattern Generator) module is a sub module of the BPG. The PGEN is responsible for reporting when data is being sent to the Aurora GTX IP, the next block address that is going to be reset from the DLPC964 with the mcp_start signal, errors that occur (timeout or DMD HSSI), and settings chosen from the user. The PGEN modules are shown in Figure 2-5 and are explained in more detail below.