DLPU133 March 2024 DLPC964
Signal Name | Input/ Output | Description |
---|---|---|
refclk_ui_p refclk_ui_n |
INPUT | Fixed 200MHz LVDS reference clock generated from DLPC964 Apps FPGA (Reference from VC-707: U51). |
reset_ui | INPUT | Push button (Reference from VC-707: SW7) to reset the DLPC964 Apps FPGA. |
irqz | INPUT | PBC Interrupt from DLPC964 Controller. |
running | OUTPUT | Goes to LED0 (Reference from VC-707 GPIO_LED_0) on DLPC964 Apps FPGA to signal when out of reset. |
C964_init_done | INPUT | Input from the DLPC964 that tells the DLPC964 Apps FPGA to be pulled out of reset. |
wdt_enablez | OUTPUT | Watchdog Timer set to '1' when in operation |
rxlpmen | OUTPUT | Set to 0 for low power mode equalization. Refer to the Xilinx App note for more information. |
ext_hssi_rst | OUTPUT | Signal that resets the DLPC964 HSSI Interface. |
hssi_bus_err | INPUT | From DLPC964 that signals there was a sync error when loading last block onto DLPC964. |
hssi_rst_act | INPUT | From DLPC964 to tell Apps DLPC964 the HSSI is being reset |
load2 | OUTPUT | Used during DLPC964 init process to setup DMD in load2 mode. |
blkmode[1:0] | OUTPUT | Used during DLPC964 init process to setup DMD superblock mode. |
blkaddr[4:0] | OUTPUT | Block (or superblock) address the issued mcp_start is sent. |
mcp_start | OUTPUT | Signals the DLPC964 to load whatever data was sent onto the DMD. |
mcp_active[3:0] | INPUT | From the DLPC964 to signal when the DMD is loading data onto the DMD. Only 4 loads can happen at once. |
blkloadz | INPUT | From the DLPC964 to signal when the block data sent is done being loaded and ready to be sent to the DMD. |
dmdload_req | OUTPUT | Signals the DLPC964 to load the block recently sent into the controller into the DMD. |
gtrx_ch0_refclk_p/n gtrx_ch1_refclk_p/n gtrx_ch2_refclk_p/n gtrx_ch3_refclk_p/n |
INPUT | Reference clock from the DLPC964 for each of the Aurora Transmit channels (GTX Channel 0 - 3). |
ch0_gtx_p/n[2:0] | OUTPUT |
Aurora 10Gbps Transmit channel 0. User-k data is sent across channel 0 ONLY along with the data. When slow mode is enabled (pbc_bpg_normal_mode_en = 0), channel 0 is the only channel sending data. |
ch1_gtx_p/n[2:0] | OUTPUT | Aurora 10Gbps Transmit channel 1. |
ch2_gtx_p/n[2:0] | OUTPUT | Aurora 10Gbps Transmit channel 2. |
ch3_gtx_p/n[2:0] | OUTPUT | Aurora 10Gbps Transmit channel 3. |
i2c_sda | INOUT | I2C Data line shared with the DLPC964. |
i2c_scl | INOUT | I2C Clock line shared with DLPC964. |
fmc_gpio[6:0] | INOUT | GPIO between the DLPC964 Apps FPGA and DLPC964. |
led | OUTPUT | Goes to LED1 (Reference from VC-707 GPIO_LED_1) on DLPC964 Apps FPGA to signal when BPG is enabled. |
testmux_uo[15:0] | INOUT | Debug mux for the DLPC964 Apps FPGA. |