There are three key benefits of
smartphone companion projectors:
- Shared big-picture
experiences. A larger image size enables a more comfortable extended
viewing experience. Rather than having to gather around a small phone screen, a
projected image enables more viewers to watch and be farther away from the
display. While a smartphone screen is typically held at an arm’s length or
closer, a smartphone companion projector (see Figure 2) can create an image size as large as 50 inches diagonally in a dim room,
enabling a viewing distance of 6 feet or more from the projection surface.
- Portability. Smartphone
companion projectors are typically small enough to easily fit in a pocket or a
bag, as shown in Figure 3. With such a small form factor, users can bring a big picture experience
anywhere they go. Battery-powered smartphone companion projectors enable
cable-free viewing experiences when a power outlet is not conveniently
located.
- Flexible viewing surfaces.
Smartphone companion projectors can use a variety of surfaces as projection
screens as long as the surface’s color, uniformity and glossiness are
acceptable. While the most common viewing surface is an interior wall, as shown
in Figure 4, ceilings or home exteriors can also be used.