SBAA274A September   2018  – March 2023 ADS1118 , ADS1119 , ADS1120 , ADS112C04 , ADS112U04 , ADS1146 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263

 

  1.   A Basic Guide to Thermocouple Measurements
  2.   Trademarks
  3. 1Thermocouple Overview
    1. 1.1 Seebeck Voltage
    2. 1.2 Thermocouple Types
      1. 1.2.1 Common Thermocouple Metals
      2. 1.2.2 Thermocouple Measurement Sensitivity
        1. 1.2.2.1 Calculating Thermoelectric Voltage from Temperature
        2. 1.2.2.2 Calculating Temperature From Thermoelectric Voltage
      3. 1.2.3 Thermocouple Construction
      4. 1.2.4 Tolerance Standards
    3. 1.3 Thermocouple Measurement and Cold-Junction Compensation (CJC)
    4. 1.4 Design Notes
      1. 1.4.1 Identify the Range of Thermocouple Operation
      2. 1.4.2 Biasing the Thermocouple
      3. 1.4.3 Thermocouple Voltage Measurement
      4. 1.4.4 Cold-Junction Compensation
      5. 1.4.5 Conversion to Temperature
      6. 1.4.6 Burn-out Detection
  4. 2Thermocouple Measurement Circuits
    1. 2.1 Thermocouple Measurement With Pullup and Pulldown Bias Resistors
      1. 2.1.1 Schematic
      2. 2.1.2 Pros and Cons
      3. 2.1.3 Design Notes
      4. 2.1.4 Measurement Conversion
      5. 2.1.5 Generic Register Settings
    2. 2.2 Thermocouple Measurement With Biasing Resistors Attached to the Negative Lead
      1. 2.2.1 Schematic
      2. 2.2.2 Pros and Cons
      3. 2.2.3 Design Notes
      4. 2.2.4 Measurement Conversion
      5. 2.2.5 Generic Register Settings
    3. 2.3 Thermocouple Measurement With VBIAS for Sensor Biasing and Pullup Resistor
      1. 2.3.1 Schematic
      2. 2.3.2 Pros and Cons
      3. 2.3.3 Design Notes
      4. 2.3.4 Measurement Conversion
      5. 2.3.5 Generic Register Settings
    4. 2.4 Thermocouple Measurement With VBIAS For Sensor Biasing and BOCS
      1. 2.4.1 Schematic
      2. 2.4.2 Pros and Cons
      3. 2.4.3 Design Notes
      4. 2.4.4 Measurement Conversion
      5. 2.4.5 Generic Register Settings
    5. 2.5 Thermocouple Measurement With REFOUT Biasing and Pullup Resistor
      1. 2.5.1 Schematic
      2. 2.5.2 Pros and Cons
      3. 2.5.3 Design Notes
      4. 2.5.4 Measurement Conversion
      5. 2.5.5 Generic Register Settings
    6. 2.6 Thermocouple Measurement With REFOUT Biasing and BOCS
      1. 2.6.1 Schematic
      2. 2.6.2 Pros and Cons
      3. 2.6.3 Design Notes
      4. 2.6.4 Measurement Conversion
      5. 2.6.5 Generic Register Settings
    7. 2.7 Thermocouple Measurement With Bipolar Supplies And Ground Biasing
      1. 2.7.1 Schematic
      2. 2.7.2 Pros and Cons
      3. 2.7.3 Design Notes
      4. 2.7.4 Measurement Conversion
      5. 2.7.5 Generic Register Settings
    8. 2.8 Cold-Junction Compensation Circuits
      1. 2.8.1 RTD Cold-Junction Compensation
        1. 2.8.1.1 Schematic
          1. 2.8.1.1.1 Design Notes
          2. 2.8.1.1.2 Measurement Conversion
          3. 2.8.1.1.3 Generic Register Settings
      2. 2.8.2 Thermistor Cold-Junction Compensation
        1. 2.8.2.1 Schematic
        2. 2.8.2.2 Design Notes
        3. 2.8.2.3 Measurement Conversion
        4. 2.8.2.4 Generic Register Settings
      3. 2.8.3 Temperature Sensor Cold-Junction Compensation
        1. 2.8.3.1 Schematic
        2. 2.8.3.2 Design Notes
        3. 2.8.3.3 Measurement Conversion
        4. 2.8.3.4 Generic Register Settings
  5. 3Summary
  6. 4Revision History

Design Notes

The measurement circuit requires:

  • Biasing resistors attached to the negative lead of the thermocouple
  • AINP and AINN inputs
  • Internal reference or an external voltage reference
  • Burn-out current sources for a separate sensor burn-out measurement
  • Isothermal cold-junction connection and measurement

Similar to the first design, this topology uses matched resistors to set the biasing for the thermocouple. In this example, matched resistors are used to bias only the negative end of the thermocouple. As long as the current through the resistors is significantly larger than the ADC input current, the resistor biasing places the negative input near mid-supply. Setting the biasing near mid-supply ensures that the input voltage is in the range of the PGA.

Attaching the bias resistors to only the negative thermocouple lead eliminates the bias current flowing through the thermocouple. This removes the error that comes from the bias current reacting with the resistive leads of the thermocouple.

Removing the bias current flowing through resistive thermocouple leads does not eliminate all errors. As in the previous topology, there is still error as the ADC input current reacts with the series input filter resistors and any series resistance associated with the input multiplexer of the ADC. Because this current cannot be removed, it is important to select an ADC with a low input current and calculate the contribution of this error to the measurement.

In the previous design, biasing resistors pulled apart the inputs in the case of a burned out thermocouple. In this design, one lead is still set to mid-supply, while the second lead is left unconnected. Because there us no current to pull up on the positive thermocouple lead, burn-out detection requires a second measurement with a change in setup for the ADC. To detect a burned out or open thermocouple, the burn-out current sources in the ADC are enabled for a separate burn-out current measurement. The burn-out current sources should not remain on for the normal measurement. These current sources, reacting with the series input filtering resistors and series resistance in the multiplexer add a large additional error.

Burn-out current sources may be set to various levels, depending on the ADC being used. Verify that the burn-out current level is high enough so that an open input creates a full-scale reading (7FFFh, assuming a 16-bit bipolar ADC) for burn-out detection.

Unless the cold junction is at 0°C, there should be a separate cold-junction measurement. This measurement can be done through several different methods, using either an RTD, calibrated thermistor, or a variety of integrated circuit temperature sensors.