SBAA274A September 2018 – March 2023 ADS1118 , ADS1119 , ADS1120 , ADS112C04 , ADS112U04 , ADS1146 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
The measurement circuit requires:
As in the previous topology, the REFOUT line is attached to the thermocouple negative input for sensor biasing. However, instead of using a resistor connected from the positive lead to AVDD, the burn-out current sources are enabled only during a burn-out sensor measurement.
There is still error as the ADC input current reacts with the series input filter resistors and any series resistance associated with the input multiplexer of the ADC. Because this current cannot be removed, it is important to select an ADC with a low input current and calculate the contribution of this error to the measurement.
To detect a burned out or open thermocouple, the burn-out current sources in the ADC are enabled for a separate burn-out current measurement. The burnout current sources should not remain on for the normal measurement. These current sources, reacting with the series input filtering resistors and series resistance in the multiplexer add a large additional error.
Burn-out current sources may be set to various levels, depending on the ADC being used. Verify that the burn-out current level is high enough so that an open input creates a full-scale reading (7FFFh, assuming a 16-bit bipolar ADC) for burn-out detection.
Unless the cold junction is at 0°C, there should be a separate cold-junction measurement. This measurement can be done through several different methods, using either an RTD, calibrated thermistor, or a variety of integrated circuit temperature sensors.