SBAA274A September 2018 – March 2023 ADS1118 , ADS1119 , ADS1120 , ADS112C04 , ADS112U04 , ADS1146 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
There are many ways to determine the cold junction temperature. RTD measurements are often used to get a more accurate temperature reading for the cold-junction measurement. There are also thermistors and other semiconductor temperature sensors that can be used to get a cold junction measurement. Regardless of how it is done, the cold-junction measurement must be accurate. Any error in the cold-junction measurement directly adds to the error in the thermocouple measurement.
Returning to the original example, assume the cold junction is measured to be 25°C. Using the K-type thermocouple table, this is the equivalent to 1.000 mV of thermoelectric voltage. To get an accurate temperature measurement of the thermocouple voltage, you would add the thermocouple voltage to the equivalent cold-junction voltage.
Now that the equivalent thermoelectric voltages have been added together, return to the table and find the equivalent temperature. With some interpolation, the resulting temperature of the thermocouple is about 623.5°C. The thermocouple voltage is non-linear and depends on the cold-junction voltage.
For accuracy, cold-junction compensation requires that the junction temperature is converted to the thermoelectric voltage for the measurement. The tables and equations start with an assumption of a 0°C cold junction. Calculation requires a specific conversion when the cold-junction is not at that temperature. As mentioned in the previous section, the proper method to calculate the thermocouple temperature follows.
A simple addition between the equivalent thermocouple temperature and the cold-junction temperature would have resulted in 625°C. This would have produced a 1.5°C error because of the thermocouple non-linearity over temperature. The only way to compensate for the non-linearity of the thermocouple curve is to convert the cold-junction temperature to the equivalent voltage, sum the thermocouple measurement voltage and cold-junction equivalent voltage, and convert the result back to temperature.
As noted earlier, if the cold-junction is held at 0°C (as if held at the temperature by an ice bath), then the equivalent cold-junction thermoelectric voltage is 0 mV. This allows for a direct conversion of the thermocouple voltage to temperature.