SBAA275A June 2018 – March 2023 ADS1120 , ADS112C04 , ADS112U04 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS122U04 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
An IDAC current source drives both the RTD and the reference resistor, RREF. Because the same current drives both elements, the ADC measurement is a ratiometric measurement. Calculation for the RTD resistance does not require a conversion to a voltage, but does require a precision reference resistor with high accuracy and low drift.
The measurement circuit requires:
First, identify the range of operation for the RTD. For example, a PT100 RTD has a range of 20 Ω to
400 Ω if the temperature measurement range is from −200°C to 850°C. The reference resistor must be larger than the maximum RTD value. The reference resistance and PGA gain determines the positive full-scale range of the measurement.
Then, choose the reference resistor and IDAC current value. Ideally, choosing the largest IDAC current provides the best performance by increasing the sensor signal above any noise in the system. However, there are several other considerations in determining the values. First, higher current may lead to self-heating of the RTD, which adds error to the measurement. Second, the reference resistance acts as a level shift for the sensor measurement. This level shift is used to raise the DC bias of the analog input signal so that the voltage is within the input range of the PGA. Generally, the analog input signal is set near mid-supply for best operation.
To verify that the design is within the ADC range of operation, Calculate the voltages for AIN1 and AIN2 and the maximum differential input voltage. Verify that VAIN1 and VAIN2 are within the input range of the PGA given the gain setting and supply voltage. Use the maximum RTD resistance based on the desired temperature measurement.
Additionally, the output voltage of the IDAC source calculated from VAIN1 must be low enough from AVDD to be within the compliance voltage of the IDAC current source. When the IDAC output voltage rises too close to AVDD, the IDAC loses compliance and the excitation current is reduced.
The reference resistor, RREF must be a precision resistor with high accuracy and low drift. Any error in the RREF reflects the same error in the RTD measurement. The REFP0 and REFN0 pins are shown connecting to the RREF resistor as a Kelvin connection to get the best measurement of the reference voltage. This eliminates any series resistance as an error from the reference resistance measurement.
The lead wire resistance is an error term in the two-wire RTD measurement. The previous calculations neglect the lead resistances, but can be added to the RRTD term.