SBAA275A June 2018 – March 2023 ADS1120 , ADS112C04 , ADS112U04 , ADS1147 , ADS1148 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1220 , ADS122C04 , ADS122U04 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS125H02 , ADS1260 , ADS1261 , ADS1262 , ADS1263
Figure 2-13 shows a circuit topology for measuring two-, three-, and four-wire RTDs using a high-side reference. There are four connections to the RTD header and five connections to the ADC multiplexer. The device is programmed differently depending on which type of RTD is being used.
The measurement circuit requires:
The IDAC always sources current from AIN0 into the first RTD connection and RBIAS is used to shift the input voltage level to near mid-supply so that the RTD measurement is in the PGA input range.