SBAA515A June 2021 – September 2022 AMC3301 , AMC3301-Q1 , AMC3302 , AMC3302-Q1 , AMC3306M05 , AMC3306M25 , AMC3330 , AMC3330-Q1 , AMC3336 , AMC3336-Q1
Figure 3-3 shows the schematic for the ferrite beads on the left and the common-mode choke on the right. Note that three ferrite beads are required, one for each input as well as one for the HGND trace to the shunt resistor. The common-mode choke has two channels and terminating the HGND connection to VINN near the common-mode choke is necessary. The differential RC filter created by R2, R4 and C12 is placed between the ferrite beads or common-mode choke and the AMC3301. Refer to the layout guidelines section in the device’s data sheet for additional detail.
The ferrite beads or common-mode choke should be placed as close to the device as possible to limit the amount of copper area that will act as an antenna. A direct and low inductance connection should be made from pin 2 (DCDC_HGND) to pin 8 (HGND). Figure 3-4 shows the recommended layouts for the ferrite beads on the left and the common-mode choke on the right.