SBAA549 April   2022 AMC23C11 , AMC23C12 , AMC23C14

 

  1.   Trademarks
  2. 1Background
  3. 2Overcurrent Protection on DC+
  4. 3DC+ Power Supply Solution
    1. 3.1 Selection of Charge Pump Capacitor
    2. 3.2 Simulation in PSpice for TI
    3. 3.3 Hardware Test
    4. 3.4 Low-Cost Power Supply Solution
  5. 4Power-On Short-Circuit Risk and Solution
  6. 5Reference

Low-Cost Power Supply Solution

The bootstrap circuit in Section 3.1 is similar to the power supply of the high-side gate driver. Through reuse, this power supply can reduce the cost. As shown in Figure 3-5, VCC is the power pin of the high-side gate driver and this solution removes a high-voltage diode (D1) and RC (C7, R6).



Figure 3-5 Low-Cost Power Supply Solution

The solution shown in Figure 3-5 increases a load for the power supply of the gate driver, so it is necessary to pay attention to the impact of the gate driver. Increasing the current-limit resistance (R4) can reduce the impact. This solution still has the limitation because the isolated comparator power supply is dependent on the half-bridge circuit operation.