DC coupled systems eliminate coupling
capacitors. The DC coupled system has the following advantages:
- Lower bill of material cost and
less board space.
- Performance degradation due to
non-linear effects in capacitors can be eliminated including THD degradation at
low frequency and board vibration effects.
- Start-up pop is eliminated..
- The ADC output is valid to DC
which allows for the possibility to do measurements such as voltage and current
for test and measurement.
DC coupling also has some
disadvantages:
- The DC biasing of the input pins
is not determined by the ADC circuit but by the external source. Since the
biasing is not always optimum, the ADC can display a reduced signal
handling.
- The Dynamic Range Extension (DRE)
functionality of the ADC relies on adapting the PGA gain. This functionality can
also be limited in DC coupled applications.
In DC coupling, DC differences between the INxP and INxM pins appear as an offset
at the output of the ADC which can lead to saturation of the ADC output at high PGA
gains. Therefore high PGA are not always possible with DC coupling.