SBAA586 October 2023 AMC23C11 , UCC23513
Simulations have been made for the circuit to drive a low side IGBT of an active brake circuit in PSpice™ for TI. Figure 4-1 shows the schematic for the simulation.
The simulation uses an AMC23C14's PSpice™ simulation model as the model of AMC23C11 is yet unavailable on ti.com. For the DESAT implementation discussed in this application note, the circuitry connected to the OUT2 (pin7) in the schematic can be ignored, and the AMC23C14 shows the same behavior as the AMC23C11 with the LATCH input (pin7) tied to low.