The following list is the startup procedure in NCO only mode:
- Start the DEVCLK
- Apply power
- Assert Reset
- De-assert Reset – Fuse ROM load will automatically begin
- Program part configuration (CH_CFG, DCM_EN, MXMODE_*, etc.) including the desired NCO configuration. Programming frequency and phase settings does not require using NCO_CHG_BLK as long as NCO_EN=0.
- Wait for Fuse ROM load to complete (FUSE_DONE=1)
- Apply SYSREF (if used) to inputs. This may have been done at any earlier point if desired, but must be stable by here.
- Set DP_EN
- If using LVDS inputs, clear LVDS_CLK_ALM & STROBE_ALM
- Synchronize the system
- If using LVDS Strobes for alignment:
- Set LVDS_STROBE_ALIGN
- Wait for LVDS_STROBE_DET=1
- If using SYSREF for alignment
- See SYSREF Windowing to enable and align synchronous SYSREF capturing.
- Set SYSREF_ALIGN_EN
- Wait for SYSREF_DET=1
- Clear SYSREF_ALIGN_EN
- If using only the NCO, it is possible to continue without synchronization if no synchronization is desired.
- Configure FIFO_DLY (this may be done early but should be complete by here)
- Set NCO_EN
- Synchronize the NCO accumulators using the method selected in NCO_SYNC_SRC.
- Clear all SYS_ALM bits
- Wait for 100 DACCLK cycles for corrupted data to be flushed.
- Enable Transmission using the TXENABLE pin or TXEN_A/B registers.
When operating only the NCO (no LVDS), the part will automatically run at some unknown alignment without aligning to SYSREF. If SYSREF alignment is desired, the user should align to SYSREF before setting NCO_EN = 1.