Under the Mac OS X operating system, select a
specific sampling frequency because the sampling frequency cannot be changed on
nearly all application software.
To set the DAC sampling frequency:
- Open the Audio MIDI Settings options (Application→Utility→Set Audio MIDI), as illustrated in Figure 4-11.
- Select the Audio Input tab in the Set Audio MIDI options group, as Figure 4-11 shows.
- Select the desired DAC sampling frequency from seven options: 8 kHz, 11.025 kHz,16 kHz, 22.5 kHz, 32 kHz, 44.1 kHz, and 48 kHz.
To set the ADC sampling frequency:
- Open the Audio MIDI Settings options (Application→Utility→Set Audio MIDI), as illustrated in Figure 4-11.
- Select the Audio Output tab in the Set Audio MIDI options group, as shown in Figure 4-11.
- Select the desired ADC sampling frequency from seven options: 8 kHz, 11.025 kHz,16 kHz, 22.5 kHz, 32 kHz, 44.1 kHz, and 48 kHz.