SBAU374A May 2021 – May 2022 DAC12DL3200
Use the following steps to open the HSDC software and load the FPGA image to the TSW14DL3200EVM:
Click OK to confirm the serial number of the TSW14DL3200EVM device. If multiple TSWxxxxx boards are connected, select the model and serial number for the one connected to the DAC12DL3200EVM. When the EVM powers up, there is no firmware loaded in the FPGA. Click the OK button on the No firmware. Please select a device to load firmware into the board. message.
In the device drop-down menu, select "DAC12DL3200_MODE2_12b_sync_istrb” as illustrated in Figure 3-6.
The setup looks as shown in Figure 3-7.