SBAU421B June 2023 – December 2023 TMCS1123
Figure 5-1 shows the schematic of the A1 sub board on the TMCS1123AEVM PCB. Only the schematic for the A1 (25 mV/A) sensitivity variant is demonstrated in this document, as all variants use the same circuit and same PCB layout. Only U1 changes from board to board. All components associated with the 25-mV/A sensitivity variants have the nomenclature "_1" appended at the end. The 50-mV/A sensitivity variants have "_2" appended, the 75-mV/A sensitivity variants have "_3" appended, the 100-mV/A sensitivity variants have "_4" appended, and the 150-mV/A sensitivity variants have "_5" appended.