SBAU466A October 2024 – January 2025 DAC39RF10 , TRF1108
The DAC can also be configured in SPIDAC Operation (NCO only mode). In NCO only mode, data streamed from JESD is ignored and DUCs inputs are driven by SPIDAC I and SPIDAC Q. This mode can be enabled when JESD Enable is set to 0, interpolation factor is greater than or equal to 2, DP Enable is set to 1, and the DAC is configured in NCO only mode. The correct combination of number of streams and interpolation factor needs to be selected to enable the desired number of DUCs and setting the desired outputs from respective DACs, as shown in Table 2-2.
In the example, all the four DUCs are enabled. DUC0 and DUC1 are routed to DAC0. DUC2 and DUC3 are routed to DAC1. If more than one DUC is routed per DAC, then the DUC data into the DAC must be attenuated to prevent the DAC from saturating.
The NCO only mode can be configured through the GUI by following steps.
Similar to SPI DAC mode, the DDS mode can be used as a lower power option. To enable DDS mode, the following steps are used.