SBOA431 September 2020 TMP1075 , TMP108 , TMP112 , TMP144 , TMP461 , TMP464 , TMP468
Figure 4-2 shows that the temperature of the CPU increases when the clock rates increase.
Figure 4-3 shows that the benchmark performance of the CPU increases when the clock rates increase.
Lastly, Figure 4-4 shows that the temperature of the CPU increases when the clock rates the benchmark scores increase.
From these figures, a 2 °C smaller safety margin can improve the benchmark score by about 4.0%.