SBOA551 June 2022 INA240
For the single-stage difference amplifier, all that is needed is the values of the internal resistors. Sometimes these values are either partially or entirely listed in data sheets. For example, Figure 6-1 is listed in the INAx181 data sheet.
"RINT" in this table represents the input resistors, and corresponds to Ri in Figure 3-1 and Figure 5-2. The feedback resistor is not listed. However, inferences can be based on the information available. For example, the feedback resistor, Rf, in INAx181A2 can be found:
Alternatively, the combined resistance of Ri + Rf can be measured. In case no resistance information is given in the data sheet, this method can be used to find the values of Ri and Rf. As an example, the total resistance turns out to be 494 kΩ for a sample INA181A2. Since the ratio of the two resistors equals to the gain, the resistance values can be calculated:
Table 6-1 shows calculated output error terms (columns titled "Err_Vref", "Err_Vcm", and "Err_Vdiff") due to finite source impedance Rx, using these measured resistance values. The external condition is: Vref_x = 2.5 V; Vcm = 25 V; Vdiff = 50 mV. The last column, "Err_Total" is the sum of all three error terms.
Rx (kΩ) | C = Rx / (Ri + Rf) | m = C / (1 + C) | Err_Vref (mV) | Err_Vcm (mV) | Err_Vdiff (mV) | Err_Total (mV) |
---|---|---|---|---|---|---|
1 | 0.0020 | 0.0020 | –5.05 | 50.54 | 0.10 | 45.59 |
5 | 0.0101 | 0.0100 | –25.07 | 250.66 | 0.50 | 226.10 |
10 | 0.0203 | 0.0199 | –49.63 | 496.35 | 0.99 | 447.70 |
20 | 0.0405 | 0.0389 | –97.34 | 973.37 | 1.95 | 877.98 |
30 | 0.0608 | 0.0573 | –143.22 | 1432.17 | 2.86 | 1291.82 |
40 | 0.0810 | 0.0750 | –187.38 | 1873.78 | 3.75 | 1690.15 |
50 | 0.1013 | 0.0920 | –229.91 | 2299.15 | 4.60 | 2073.83 |