Differential signals rely on the high common-mode rejection of differential amplifier circuits to reduce noise and other errors. This application note explores the relationship between resistor tolerance and common-mode rejection in difference amplifier circuits. Equations are derived to determine the common-mode rejection ratio (CMRR) of a differential amplifier circuit as a function of absolute resistance, resistor tolerance, or matched ratio tolerance. The precision ratiometric matching of the RES11A-Q1 thin-film resistor divider pair can improve the effective CMRR of a difference amplifier circuit.
All trademarks are the property of their respective owners.
A differential voltage signal is defined as the difference in voltage between two signal-carrying traces. Often these signals are balanced, meaning that the two signal voltages are equal in magnitude but of opposite polarity, as shown in Figure 1-1. The differential voltage (VDiff) can be resolved by subtracting the positive signal voltage from the negative signal voltage as shown in Equation 1.
This subtraction function is one of the main benefits of differential signaling, as the subtraction function removes unwanted common-mode voltages from the signal chain. A common-mode voltage (VCM) is a voltage that is present on both signal traces, that is equal in both magnitude and polarity. In differential circuits, VCM is defined as the average of the two signal voltages, Equation 2.
These unwanted common-mode voltages can be in the form of noise, or as a DC bias from the previous signal stage. Unlike the signal voltages which are of opposite polarity, these common-mode voltages are rejected by the subtraction function defined in Equation 1. The following figures illustrate this principle for both AC and DC common-mode voltages.
In practical electrical circuits the common-mode voltage is not perfectly removed from the differential signal, however it can be significantly attenuated. The magnitude of the common-mode attenuation is determined by various non-idealities in the circuit, as discussed in the following sections.