SBOU122B September 2013 – August 2016 INA118 , INA121 , INA122 , INA126 , INA129 , INA141 , INA155 , INA156 , INA188 , INA317 , INA818 , INA821 , INA828
Figure 8 shows an example of how to set up the EVM for single-supply operation with a direct voltage connection to the reference (REF pin).
The following connections were made:
Note that C9 and C10 are prepopulated with 0.1-µF power-supply decoupling capacitors. It is not required to remove C9 for proper single-supply operation. Refer to the device data sheet for additional power-supply decoupling information.