SBOU246 January 2022 TMP61 , TMP61-Q1 , TMP63 , TMP63-Q1 , TMP64 , TMP64-Q1
The simplest construction of the NTC thermistor-based temperature sensing network is the one shown in Figure 2-1. For the ADC, we will use 12-bit resolution and a reference voltage of 5 VDC. The 12-bit resolution is an acceptable resolution for measurement while the 5 VDC reference voltage simplifies power rail requirements. These design decisions result in the voltage response shown in Figure 2-2.
While this voltage-biased network is very simple, reducing the bill of materials cost required. The temperature output VTEMP shows non-linear behavior at the temperature extremes.