SCDA047 January 2024 TMUX1108 , TMUX1119 , TMUX121 , TMUX136 , TMUX1574
Passing a signal through two or more multiplexers in series, often called cascading, can be used as a creative way to realize unique system designs that otherwise are not possible. While there are a wide range of circumstances that can see a designer implement cascading multiplexer in a system, there are two main instances where this implementation is used the most.
The most common situation where cascading multiplexers are used is in configuration expansion, where smaller multiplexers create a larger multiplexer with a greater number of inputs feeding into the eventual single output. Alternatively the opposite flow can also be done where many outputs feed into a single input as well. An example is highlighted below in Figure 1-1 where 3 SPDT (2:1) multiplexers are used to create a 4:1 multiplexer.
The other most common instance where a multiplexer can be cascaded is commonly called a ‘cross-point switch’. A cross-point switch is a switch that allows any input to find a path to any other input or output without interferences from any other signal path. For example, on the right in Figure 1-2 we see a type of cross-point switch called a switch array that is created by cascading many multiplexers. Here, Ain can be connected to any of Aout, Bout or Cout, depending on the logic of each multiplexer. At the same time, Bin can also be connected to any of the three outputs, given the correct logic implementation on your multiplexers, without having to be shorted to Ain at the same time. In this example, while a small array can be created by simply shorting the outputs of a couple multiplexers together and utilizing control logic efficiently without cascading (Left image in Figure 1-2), as you increase the size of the array, you can use smaller multiplexers for flexibility in PCB-routing and logic control while also limiting certain parasitics, which we explore in more depth through this report.
With cascading multiplexers, there are a few behavioral specifications that accumulate as more multiplexer stages are added. How these affect the system varies depending on how these multiplexers are being used in a given system. We’ll examine these specifications in the following section.